Part Number: TPS61040 Tool/software: Hi,
I'm planning to use TPS61040 for my below requirement:
These are the inputs I've given to Webench.
VIn(Min)= 4.8V
VIN(Max) = 5.5V
Vout=7V
Iout(Max) =50 mA but typical would be very small around 10mA…
Part Number: TPS61040-Q1 Tool/software: We are planning to register your product TPS61040QDBVRQ1 in the IMDS (International Material Data System) .
Could you please advise us on the procedure to initiate the IMDS registration for this part?
If we…
Part Number: TPS61040 Other Parts Discussed in Thread: BQ27510 , TPS61027 , TPS61046 , BQ25120A , Please confirm whether the following parts belong to Commodity Interface IC Chip, or Gate Driver IC Chip?
P/N
Description
BI MFR
BI MPN
BI…
Part Number: TPS61040 Other Parts Discussed in Thread: TPS61041 Tool/software: Hi, I have used TPS61040DBVR to deliver 6V to the transistor on board powered with 3V battery. The transistor is used as a switch for my circuit. Once I put in the battery…
Part Number: TPS61040-Q1 Other Parts Discussed in Thread: TPS61040 Tool/software: Hello,
during the temperature evaluation of the TPS61040Q1 actual device, a uncertain behavior of the IC was observed.
In this situation, the efficiency drops sharply…
Part Number: TPS61040-Q1 Other Parts Discussed in Thread: TPS55340 , TPS61040 Hello,
I wanna design Boost circuit to increas voltage to 28V by using 5V.
in case of TPS61040-Q1, possible output voltage is 28V at maximum according to datasheet.
…
Part Number: TPS61040 Hi
I am using following part from TI
TPS61040AQDBVRQ1
I am using this part in my design for the display powering section, while testing in the RI test I am getting display flickering at 310MHz.
and one more thing less than…
Part Number: TPS61040 Other Parts Discussed in Thread: TLV61046A , TLV61048 Tool/software: Hi,
I'm planning to use TPS61040DBVR for below requirement
VIn= 4.8V
Vout=7V
Iout=100 mA
But webench power designer is not allowing me to change the current…
Part Number: TPS61040 I am trying to to run the circuit attached but the output voltage is not what is expected. I created the model with the proper capacitors and it stills outputs the same incorrect voltages. I believe there is something wrong with…
Part Number: TPS61040-Q1 1) What is the PSRR value(Frequency 10Hz to 10Mhz) for the Boost converter?.
2) We are trying to measure the PSRR value. Note : The input voltage is 3.3V & Output voltage is 6V
Our test set up is injecting noise (Modulating…