Part Number: TPS61040-Q1 Other Parts Discussed in Thread: TLV61047 Tool/software: We are using the TPS61040-Q1 to supply power to a rear-view camera as follows:
Vin = MAIN_5V = 4.05V
Vout = REAR_PWR = 9V
Load current (when REAR_PWR is…
Part Number: TPS61040-Q1 Tool/software: We are planning to register your product TPS61040QDBVRQ1 in the IMDS (International Material Data System) .
Could you please advise us on the procedure to initiate the IMDS registration for this part?
If we…
Part Number: TPS61040-Q1 Other Parts Discussed in Thread: TPS61040 , TPS61170 Tool/software: Hello
i need to build 2 white leds circuits with PWM control, one with 6 leds and the second with 8 leds, with max current of 20mA.
i found TPS61040 ic which…
Part Number: TPS61040-Q1 Other Parts Discussed in Thread: TPS61040 Hi Team,
I have some queries on the TPS61040-Q1 IC.
1. What is the max. load current support by TPS61040-Q1 IC?? In datasheet, I saw Ilim = 450mA (MOSFET current limit) and Switch…
Part Number: TPS61040-Q1 Other Parts Discussed in Thread: TPS55340 , TPS61040 Hello,
I wanna design Boost circuit to increas voltage to 28V by using 5V.
in case of TPS61040-Q1, possible output voltage is 28V at maximum according to datasheet.
…
Part Number: TPS61040-Q1 Other Parts Discussed in Thread: TPS61040 Tool/software: Hello,
during the temperature evaluation of the TPS61040Q1 actual device, a uncertain behavior of the IC was observed.
In this situation, the efficiency drops sharply…
Part Number: TPS61040-Q1 1) What is the PSRR value(Frequency 10Hz to 10Mhz) for the Boost converter?.
2) We are trying to measure the PSRR value. Note : The input voltage is 3.3V & Output voltage is 6V
Our test set up is injecting noise (Modulating…
Part Number: TPS61040-Q1 Other Parts Discussed in Thread: TPS61040 Can you please explain what is the difference between TPS61040 A QDBVRQ1 and TPS61040QDBVRQ1? Both parts seem to have the same data, but different top side marking. So, what is that A…
Part Number: TPS61040-Q1 Other Parts Discussed in Thread: TPS61040 Hi,
we are using the TPS61040-Q1 Boost converter for converting the 3.3V to 6V. Please find the schematics
Attached the power sequence of this converter
The Yellow color represent…
Part Number: TPS61040-Q1 Hi ,
Can I place the feedback circuit behind the capacitor C2, as indicated by the red line below,What are the risks if i do this, how do you suggest to place it reasonably? Tks