Other Parts Discussed in Thread: TPS61045 , TPS61040 , TPS61041 HI,
I have tried to run the pspice transient model on orcad 16.6.However when i simulate the circuit it give me this error.
----------------------------------------------------------------…
Other Parts Discussed in Thread: TPS61045 Hi,
I am currently working on an adaptive power system which requires to use TPS61045. I am just wondering, is there any information related to the time taken to to boost up the voltage with the control signal by…
Other Parts Discussed in Thread: TPS61045 Just a quick question. In this IC there is a control pin which allows user to control the output voltage. Is there a range limit to how much the output voltage can sweep across? If I set R1, R2 and R3 correctly…
Other Parts Discussed in Thread: TPS61045 , TPS61080 , TPS61081 Looking for a single output boost transducer power supply. 5V input with firmware programmable output of 5, 10, 15 or 24V. 40mA max. output current. Was intrigued by digitally adjustable boost…
Other Parts Discussed in Thread: TPS61045 , TPS61042 , TPS61043 , TPS61040 Quick question on the TPS61045. The design I am working with will need the un-boosted voltage to pass through the boost regulator when not active. Is is possible to place a diode between…
Other Parts Discussed in Thread: TPS61045 , TPS61040 Hi,
Currently i need a boost converter that has the functionality of controlling the output voltage. I know TPS61045 has a digital control pin for me to adjust the output voltage. However, the process…
Other Parts Discussed in Thread: LMR64010 , LM5000 , LMR62421 , TPS61045 , LM5001 I am looking for a 5V to 24V dc-dc converter. From the step up converter list, I got
LM5000, LMR62421, LMR64010.
When I tried to simulate this in web bench, none of them were…
Hi Eric,
When applying another voltage through a resistor connected to FB pin, the current proportion in R1 and R2 changes. In this way, the output voltage can be changed. You can refer to the datasheet of TPS61045 for detailed information, it just uses…