Part Number: TPS61046 Other Parts Discussed in Thread: TPS61372 , TPS61086 Hi Team,
Can you help to check if we have any devices spec similar to TPS61046, but with Force PWM mode only to reduce output ripple? Thanks.
Part Number: TPS61046 Other Parts Discussed in Thread: TLV61046A , TPS61040 Hi team,
I'd like to find a boost device that can support below conditions. I can see TPS61046 is suitable and I just want to check if there is another suitable device.
Vin…
Part Number: TPS61046 Hi team,
My customer was wondering more about this over-voltage protection feature.
If the output voltage exceeds the 28V condition, does this mean the output is effectively disconnected from the load? Does it produce any output…
Part Number: TPS61046 Hi Team,
From the datasheet, we can see there is a Internal 10-ms Soft Start Time, is there a range? and why is a segment of the waveform horizontal during soft start?
Thanks.
Best regards,
Hailiang
Part Number: TIDA-00462 Other Parts Discussed in Thread: CD4049UB , TPS61046 , LMP7715 , DIP-ADAPTER-EVM , MSP430FR5969 , TLV61046A
Dear TI Team,
We want to design 'TIDA-00462'.
Following TIDA-00462 user guide, I purchased the parts as below.
TPS61046…
Part Number: TPS61046 Hello,
My situation: Input = [+4,8V / +5,2V] Ouput = [+6V] Consumption = 0,05A
When I try to use webench for these conditions I have a message as: "Design update failed. Duty cycle is lower than the minimum for this device"…
Part Number: TPS61046 Other Parts Discussed in Thread: TPS61251 , TPS61086 , TPS61093 Hi,
I tried designing a boost circuit using TPS61046 with TI Webench tool using conditions Vin(min) 2.1V, Vin(nom) 2.5V, Vin(max) 2.9V, Vout 6V. For Iout I tried 0.12A…
Part Number: TIDA-00462 Other Parts Discussed in Thread: MSP430FR5969
Dear TI Team,
We want to design 'TIDA-00462'.
Following TIDA-00462 user guide, I purchased the parts as below.
TPS61046YFFR
TSP7133DSER
CD4049UBNSR
LMP7715MF/NOPB
But the parts…
Part Number: TPS61046 Other Parts Discussed in Thread: TPS61251 , TPS61086 , TPS61093 , LM2623 , LM5157 , TLV61048 , TPS61087 , TPS61022 , TPS61288 Hello TI experts,
I am going to suggest TPS61046 to my customer, please check their condition.
input : 1.9V ~ …
Part Number: TPS61046 Dear Team,
There is good new that we DIN the TPS61046 in customer's new project.
Could you help to review the schematic?
We appreciated your great support!
Many Thanks,
Jimmy