Part Number: TPS61046 Other Parts Discussed in Thread: TPS61023 , TPS61099 Hi there! I would like to have your opinions on using the TPS61046 slightly out of specification.
The input voltage is between 3.0 V and 3.3 V, the output voltage is set to 3.71…
Part Number: TPS61046 Hi Team,
I would like to find the solution which meet below requirement . I find TPS61046 in ti.com. Do we have more appropriate solution? or next gen roadmap could send me directly?
Description
Vin
Vout
Iout
Efficiency…
Part Number: TPS61046 Other Parts Discussed in Thread: , TPS61372 Light load regulation is not so good.
I would like to stabilize the output voltage of at least 10mA.
Is there anything else you'd recommend?
(Condition)
4.2Vin
Setting output voltage…
Part Number: TPS61046 Hi team,
I found there is one contradiction about the operation temperature from the TPS61046 datasheet. Could you please tell me which one is correct, -40~85C or -40~125C? Thanks!
Best Regards
Zhengquan Lu
Part Number: TPS61046 Other Parts Discussed in Thread: TPS61070 Hi TI Experts,
We are developing a boost converter circuit using TPS61046 which powers an OLED display. Refer below circuit for reference. We observed that as soon as EN is driving high,…
Part Number: TPS61046 Hello E2E,
I have an urgent customer question that I am hoping you can help me with. They are wondering if the TPS61046 will be stable with 4x22uF capacitors with the following specs.
Vin min = 2.5V
Vin max = 5V
Vout = 12V (can…
Part Number: TPS61046 Tool/software: WEBENCH® Design Tools Hi team,
I'm trying to simulate this part on Webench with the following parameters-
2.5-3V in, 22V out, 100 mAload max.
But when I simulate it I get an error that the device doesn't work with…
Hi Charlie,
TLV61046A and TLV61048 are not p2p compatible. So please don't just drop in the TLV61046A instead of the TLV61048.
Following is the schematic for generating +/-25V based on TPS61046, which applies to TLV61046A as well.
The diode D7 and D8…
Hi Abdul,
I assume that you are looking for a device with load disconnect at typical voltage.
TPS61046 is fit for the load disconnect function.
TPS61046 28-V Output Voltage Boost Converter in WCSP Package datasheet (ti.com)
Please tell me if you have other…
Part Number: TPS61046 Hi My customer has question.
Customer want to set aVout=28V. However, the output voltage is only set to 24V. In addition, I tried to set again 20V, 22V, 24V, 26V, 28V. 20V and 22V become the output voltage of each value normally. But…