Other Parts Discussed in Thread: TPS61050 URGENT!!
customer has problem to operate the TPS61050EVM. See attached screen shoot.
Note the red message: ”TPS61050 is Not Operational”
However, he can write and read registers
The LED itself does…
Other Parts Discussed in Thread: TPS61050 , TPS62150 , TPS92510 , LM3405 Hi,
We have an application for a single white light LED driver. LED specs: Vf= 2.9 - 3.3V. If = 150ma. - 700ma. Must be constant current output.
The selected current output must remain…
Other Parts Discussed in Thread: TPS61050 Hi~
Does TI has the Source code of TPS61050 EVM Software?
Could you release the source code of TPS61050 setup.exe?
Thanks..
Hi ,
I just changed to TPS61050 EVM for 450mA/ 500mA testing under the Torch mode .
As I know that attachment should be operate 450mA/ 500mA,
But It did not work at 450mA/ 500mA.
separated Power supply is added for this EVM.
If you have some debugging…
OK. What I want to say is...
Less than 100mA was just test condition. I'm using that not only less than 100mA, but also 1000mA.
So, TPS61050/1 couldn't be a solution.
Anyway, I think that you don't have a ripple data in PSM.
I've ordered EVM…