Part Number: TPS61087EVM-317 Hi,
I have tested here TPS61087EVM-317 board and I applied 3.5V input and 15V output with 36ohm load.
Everything work for about 1minute after that ouput start oscillating 15Volts on the output. Seems like thermal shutdown…
Output voltage 10V +- ripple as on oscillograph
Input on feedback over additional 18k ohm resistor 1.58V
with board TPS61087evm-317 @650kHZ
Any help are welcome
Thanks
Hi Fergus,
Thank you for your comment.
I tested 200Hz PWM signal on EN port using our EVM. but there is also a audible noise. so I think this is not layout problem.
If you have TPS61087EVM-317, would you please test this issue using our EVM?
1…