Part Number: TPS61088 Tool/software: Hello guys,
One of my customers is considering using TPS61088 for their next products.
They'd like TI to check their schematic. But they don't want to disclose their schematic on this thread.
So could you please…
Part Number: TPS61088 Other Parts Discussed in Thread: , , TPS61288 , Tool/software: Hi TI,
I am looking for a power supply that can output about 4.5A at 9V with an input voltage range of 5V to 8.4V. I plugged these numbers into WEBENCH and the top suggested…
Part Number: TPS61088 Tool/software: Hello
We use TPS61088 to convert 5V to 7.2V. This is out circuit:
This is our PCB Layout:
Recently we met a issue when doing Damp Heat/High Temperature operating test: the output of this circuit suddenly drop to 4…
Part Number: TPS61088 Tool/software: Dears,
My customer are using TPS61088 as a boost circuit, and there is a probability that TPS61088 cannot be boosted on the client side, resulting in abnormal voltage output and the output voltage being the same…
Part Number: TPS61088 Other Parts Discussed in Thread: TPS25940 , Tool/software:
See TI has a combination of TPS25940 and TPS61088 SSD backup scheme, would like to ask whether TI has a similar integrated IC at present?
Part Number: TPS61088-Q1 I am trying to design TPS61088-Q1 with following design inputs
Vinmin=3.2V Vinnom=3.3V Vinmax=3.4V Vout=5V Iout=3A Ta=100C
Due to Ta=100C switching frequency is coming 195.367 KHZ and Tj=129.646C
Is this design OK ? I am attaching…
Part Number: TPS61088 Hello sir
When I use TPS61088, input voltage is 7.92V. when the enable pin is high,the output voltage is 12V. this is right.
But when the enable pin is low, the output voltage is 7.63V which is expected to be zero. why does this…
Part Number: TPS61088 Tool/software: Hi TI teams,
We used TPS61088RHLR to convert 5V to 7V. When my customer did soak test, the output suddenly drop to 4.4V after 3 days and can recover after power cycle. This issue happened twice, the second time was 7…
Part Number: TPS61088-Q1 Hello team,
my customer has questions for TPS61088-Q1 (RHL0020A).
1. How long is a. in millimeters?
2. is b. (0.2) max value or typ valu?
best regards,
kazusa suzuki