Part Number: TPS61088 Hi ,
Good day,
We are using TPS61088RHLR for converting a battery output (3.6V) to 5V.
Attaching the Screenshot of the implemented circuit below
In this, the Vin is taken from Battery. During the normal operating condition, (ie…
Part Number: TPS61088 Hello TI Team.
I used TPS61088 Boost IC in Our Project ,
Requirement:
Input=3S1P Li-ion Battery pack (11.1V).
Output =12V/1.8A,
Quarry:
1) Suggest FB pin resister Divider network value and how much voltage should be set at FB pin…
Hi Allen,
Both two bode plots look strange, could you please check whether the wire connection or measurement is correct? The bod plot should be similar to the calculated one in the excel tool. Or maybe you can use another DCDC EVM to check the connection…
Part Number: TPS61088 Other Parts Discussed in Thread: LM5175 , TPS55289 Hi Team,
Our customer would like to limit the output current of their custom made board with TPS61088 to 1.4A and would like to confirm if it is possible using the ILIM pin. I understand…
Part Number: TPS61088 Hi,
For a new product I'm using the TPS61088RHLR boost converter. However, when testing the output voltage for different loads, I noticed that that when the load drops from 5V 3A to 0A, there is quite a big overshoot which I was…
Part Number: TPS61088 Hi,
I have attached the schematic for review. inpur voltage is 5V and output required is 3A@11V.
Kindly provide feedback.
QSB SCM 14032022 -TPS61088RHL.pdf
Part Number: TPS61088 Hi,
I have attached the schematic for review. inpur voltage is 5V and output required is 3A@11V.
Kindly provide feedback.
8037.QSB SCM 14032022 -TPS61088RHL.pdf
Part Number: TPS61088 Hi, TI expert
There is a request for a review of the schematic applied with the boost IC (TPS61088) from the customer. (See attached schematic below)
4130.Schematic.pdf
Please review the schematic to see if there are any corrections…
Part Number: TPS61088 Hello expert,
I would like to double check if we have solution could implement 2cell battery boost to 150V application? Thanks a lot!
Best regards,
Ann Lien
Part Number: TPS61088 Other Parts Discussed in Thread: TPS61022 Hi All,
We are looking for a product with ripple noise of 100 mVpp or less under all load conditions, including the following conditions.
Input Voltage: 2.9-4.3V Output Voltage: 5.1V Output…