Part Number: TPS61088EVM-677 Tool/software: We conducted the EVM test for 3.3V to 12V output at 8W load and noticed that the efficiency is not within the desired range, at only 72% when the same inductor (1.2uH) used in the EVM board. We tried replacing…
Part Number: TPS61088EVM-677 Tool/software: TPS61088EVM-677 evaluation board - Test Results .xlsx
The EVM board was tested initially for a 9V output without any modifications. The test result is attached.
If the load increases the output voltage slightly decreases…
Part Number: TPS61088EVM-677 When I test the feedback loop of the circuit. I found the waveform had a significant jump after 10KHz both in Magnitude and phase.
Do you have any comments on this or how can I get a better result for the bode plot?
Part Number: TPS61088 Other Parts Discussed in Thread: , , TPS61288 , Tool/software: Hi TI,
I am looking for a power supply that can output about 4.5A at 9V with an input voltage range of 5V to 8.4V. I plugged these numbers into WEBENCH and the top suggested…
Part Number: TPS61088EVM-677 Hi, Good day. I hope you are well. Our customer is using the TPS61088EVM-677 and they also want to have the design files for it. They prefer the Altium files. We would appreciate if you could help us provide these files. …
Part Number: TPS61088EVM-677 Other Parts Discussed in Thread: TPS61088 the tps61088 evm board can't output more than 2A current, I just changed the feedback resistor to achieve 5V boot to 11V, when load is heavy, output voltage is not correct, and also…
Part Number: TPS61088EVM-677 We are using TPS61088RHLR evaluation board. This board should provide 9V, 3A output for a input voltage of 3.3V. But we are observing that, If the load current is increased beyond 1.2Amps , The output collapses to 5V with…
Part Number: TPS61088EVM-677 Other Parts Discussed in Thread: TPS61088 When the output load of TPS61088 exceeds 5W, the switching frequency fluctuates between 580 and 400K,
which is unstable. The parameters are as follows: Input: 3-4.2V Output: 6.1v 1…
Part Number: TPS61088EVM-677 Hi Sir/Madam,
Is it possible to advise the board size of TOS61088EVM-677?
Is it possible to share the gerber file for the EVM?
Thanks.
Part Number: TPS61088EVM-677 Other Parts Discussed in Thread: TPS61088 I tested to drive a servo motor and test stall current yesterday: with and without TPS61088 DC/DC boost.
The test with DC/DC boost from 3.2v(lab power supply output) to 6.5v(modify…