Part Number: TPS61088Q1EVM-037 Hi
Please can you provide the CE/EU Declaration of Conformity for TPS61088Q1EVM-037?
The product is CE marked but the CE/EU Declaration of Conformity is not available on the T.I website,
Thank you
Hi Ethan,
The device can work at Vin=1.2V and Vout=8V 0.75A.
the test is based on EVM parameters.
TPS61088Q1EVM-037 Evaluation Module User's Guide (Rev. A)
Connect SVIN with Vout and change R1 to 316k
Best Regards,
Fergus
Hi oneil,
The device TPS61088,TPS61088-Q1 and TPS61288 are all fit for your application.
TPS61088-Q1 is AEC-Q100 qualification, and its current limit configuration is different from TPS61088.
Other than that, the two are same.
TPS61088Q1EVM-037…
Hi Pranjali,
Thank you for reaching out.
Your design link is not available.
It is ok for your design but usually we choose our lowest switching frequency to be 200kHz.
For the Layout copper thickness, you can refer to our EVM board.
TPS61088Q1EVM…
Hi, Paul,
As for your question about evaluation boards, we sell them on our website:
http://www.ti.com/tool/TPS61088Q1EVM-037
I hope these can help you validate your design.
Is it safe to assume that the TPS61088Q1EVM-037 kit has the same layout at PMP9778, and the proposed WebBench layout, since TI engineers would want the same low emissions result?
Also - do you think that WebBench will eventually have the ability of…