Part Number: TPS61093 Hi,
Customer has an issue with inductor Acoustic Noise.
Input voltage : Max 150mAh@ Alkaline Battery 2.0~ 3.2V
Output voltage : 17V
Output current : 15 ~ 20mA
Changes to Inductor 10uH products do not remove Acoustic Noise…
Part Number: TPS61093-Q1 What is the min or max soft-start time supported by the IC.
Can the soft-start time reach as high as 100ms, if I put a 1uF cap on the SS pin?
Best Regards,
Mithun
Part Number: TPS61093-Q1 Hi team,
My customer acceptable for voltage fluctuation on TPS61093-Q1.
In datasheet, voltage changes nearly 500mV when load change.
Is there any way to suppress this fluctuation?
Regards,
Youhei MIYAOKA
Part Number: TPS61093-Q1 Hi team,
My customer have questions about 9.2.1 15V Output Boost Converter in datasheet.
1. How much RV required for C3.
2. Is it possible to add snubber circuit even diode integrated.
3. In 7.3 Recommended Operating Conditions…
Part Number: TPS61093 Hi,
My customer does not required discharge function. What device is recommend with TPS61093 without discharge function? Please advise us.
His requirement spec is as follows:
Vin 1.5V-3V
Vout 12V
Current Min 100mA
No…
Part Number: TPS61093 Hello
Does TPS6109 support 5V and 1A output current when is Vin =0 (power from capacitor)?
IF not, can you recommend an alternate solution?
Thank you
Part Number: TPS61093 Hi there,
I use TPS61093 for setting output voltage 8.0(tolerance±0.3V).
When output voltage comes from other unit, and its value is 8.4V above the setting output voltage, what will happen.
IC is damaged? or break?
…
Part Number: TPS61093
Hi Team,
In TPS61093 datasheet, it could realize the overcurrent and overvoltage protection.
As for overvoltage protection, how could it realize?
Sorry I missed it, I have checked in WEBENCH power supply Design bench,and Simulated the TPS61093, it can safely deliver 200mA. If any improvements from the design, please suggest.
Part Number: TPS61093 Other Parts Discussed in Thread: TPS61094 , TPS63900 , , TPS22917
somehow the model for TPS61094 is not added correctly to pspice for TI.
I tried to download the encrypted model and add to pspice for TI placing the file in the…