Part Number: TPS61093 Hi Team,
Our customer would like to know the scatter plot of Vref.
We understand that the min/typ/max values of Vref are is mentioned in datasheet.
However, they would like to know the scatter plot of the average value and standard…
Part Number: TPS61093 I have a TPS61093 converter, DFN package.
Top marking says:
OAP
TI
76PS
Inputting any or all of these package markings returns ZERO results for anything. I suspect TI's package marking search needs to be fixed. Did search ever…
Part Number: TPS61093 Hi,
I'd like to verify the input current for TPS61093:
Test condition as below: Vin = 3.3V Vout = 5V Iout = 0.8A
I tried used WEBENCH to simulate the above test condition by setting the Iout 0.3A (0.8A exceeded the switching current…
Part Number: TPS61093 Hi, Let me talk about the Cff calculation formula. The data sheet has the following description.
''When the output capacitor is increased to 100 μF, then the fP is reduced to 10 Hz.
Therefore, a feed-forward capacitor of…
Part Number: TPS61093 Hi, Let me talk about the settable output voltage of TPS61093. For sudden change in specifications, customer want to set the output voltage to 18V. I got two questions from customers. ・Is this device capable of outputting 18V? (It is…
Part Number: TPS61093 I have an application in which I am striving for a 5msec soft start time for the TPS61093.
I am using the reference design with Css = 47nF and Rss = 10k. With these components in place the TPS61093 does not produce the desired output…
Other Parts Discussed in Thread: TPS61093-Q1 Hi
My customer will use TPS61093-Q1 under Vin=3.3V, Voiut=5V.
But calculation method of Iout_max isn't written in that datasheet.
Are there the reference materials or calculation methods of Iout?
Best regards…
Other Parts Discussed in Thread: TPS61093 Hi, Could you tell me about TPS61093 startup sequence. Customer is trying to start up in the following order. 1.EN pin high 2.VIN pin voltage applying Is it safe to ''voltage applied to EN before VIN?
Best regards…
Other Parts Discussed in Thread: LM2623 , TPS61093 [ TPS61093 / LM2623 ] Boost Output Current Regulation
Dear Expert, My customer tries to implement the output current regulation with discrete components for TPS61093 and LM2623. (why two devices? for comparison…
Other Parts Discussed in Thread: TPS61093 Hi team,
a customer of mine has a problem with Pspise simulation of TPS61093 with EN pin.
It works good when he gives high (1 logic=Vcc) to EN pin and when going to low (0 logic=GND) but when he gives again high…