Part Number: TPS61096A Hello,
What is the functionality of VOSNS pin in TPS61096A boost converter. Is it for remote sensing for taking the feedback from load?
Please explain what it is and what are its functionalities / advantages? Thanks in advance. …
Part Number: TPS61096A Hello Team,
Is there any information regarding to the forward voltage drop of the integrated diode? Would like to have a better understanding of the output voltage with this IC is disabled.
Part Number: TPS61096A Other Parts Discussed in Thread: LM5002 Hi Sir
May we have TPS61096A road map that will more high output voltage?
And customer best efficiency for Vin=3.6~4V Vout 30V Iout<2mA
Vin=3.6~4V Vout 50V Iout…
Part Number: TPS61096A Hello, For a new design, the reference TPS61096A matchs all our requirements except the negative temperature. On the datasheet, the minimun operating is at -40°C. Our design requires -55°C What could occurs at -55°C? Have you…
Part Number: TPS61096A Other Parts Discussed in Thread: BQ25504 I have bq25504 evaluation board which energy harvests from indoor light using a small solar panel. I am going to feed the harvested energy to a smoke alarm at 10V to replace the usual 9V…
Part Number: TPS61096A Other Parts Discussed in Thread: TLV61046A Hi,
Sorry to bother, but we face some strange issue in our TPS61096A based design. We have recently got out of production few boards in which we attempt to use TPS61096A to generate stable…
Part Number: TPS61096A Other Parts Discussed in Thread: TLV61046A Hello~
Vin is 5V,and I need TPS61096A boost to 12V or 13V for PMOLED panel driving power supply.
1.To simply achieve 12V output,the three pins FB,EN,VIN are connected toghter. Is it OK or not? I…
Part Number: TPS61096A Other Parts Discussed in Thread: TPS61372 , Hi,
I have a customer that is using the TPS61069A device with:
VIN: 4.2V
VOUT: 14V
ILIM: 0.15A
They are trying to choose the inductor value (started with 2.2µH) and the calculated max…