Part Number: TPS61096A Hello,
The TPS61096A is being used for a 5V to 28V conversion.
When the 5V is supplied from an Arduino Leonardo (which is powered by 8V and provides 5V via a NCP1117 LDO), the device is destroyed and it appears the low side FET…
Part Number: TPS61096A Other Parts Discussed in Thread: TPS65192 , TPS65190 , TPS65197 Hi,
I am looking solution to shift voltage from 3.3V to 25-30V and I found this part. Because I also need DC/DC converter it will be ideal. But I need 3 or 4 level shifters…
Part Number: TPS61096A Hello!
This device integrates power converter and two level shifters. Also, this device has enable/disable function, controlled by EN pin.
Unfortunately there is no clear information in datasheet if EN pin controls this level shifters…
Part Number: TPS61096A Other Parts Discussed in Thread: TLV61046A Hi,
We integrated this part onto our circuit and found that the shutdown voltage is 2V, and when I connect a resister across, the current flows, and it stays at 2V.
May I know what is the…
Part Number: TPS61098 Other Parts Discussed in Thread: TPS61096A Hi Sir
Because TPS61096A isn't release yet, may you pls help check circuit?
Bogey 6076.boost.pdf
Part Number: TPS61096A Hi Sir
My customer use TPS61096A at Vin:4V Vout 20V Iout around 1mA. but find the output seem have some noise.
Is it normal? may you have suggestion to filter it?
Bogey
the TPS61096A has very small quiescent current which can be always on, but its load capability is only 25mA level from alkaline batteries, depending on the minimum battery voltage. what is the loading, why it need 50mA?
It sounds you need low Iq devices which minimize the drainage of your battery during sleep. You may consider TPS610986 for your 3.3V rail, and TPS61096A for your 12V rail. I also notify our experts of these devices and they may add comments.