Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: TPS61098 Hi
There is RIN resistor between SW and VIN. How can we calculate the value of RIN?
Is RIN=470ohm possible?
Best Regards,
Koji Hamamoto
Part Number: TPS61098 Other Parts Discussed in Thread: TPS61089 Hi,
I am using TPS61098 to boost voltage from LiFePo4 battery (3.2V to 2.9V) to 6 volts to drive this motor: Thomas G6/02-8
The motor draws 0.5A - 1A of current
My schematics are below, the…
Part Number: TPS61098 Other Parts Discussed in Thread: TPS61096A Hi Sir
Because TPS61096A isn't release yet, may you pls help check circuit?
Bogey 6076.boost.pdf
Other Parts Discussed in Thread: TPS61098 Hello ti community,
I'm using TPS61098 to power a microcontroller and LCD. I was thinking of changing the inductor that comes with the kit because it has a lot of dc resistance (168mOhms I was able to find inductors…
I don't think I mentioned the TPS61098 in this post but looking through the specs, it seems that TPS63900 is a good candidate. Even though I don't necessarily need the double voltage feature. Thank you for your help Nathan. Best regards,
JB
Other Parts Discussed in Thread: TPS61098 We use step files in our PCB design software to help validate PCB's. If you have a 3D model for TPS61098, I'd love to have it.
Part Number: TPS610986 Other Parts Discussed in Thread: TPS61098 hi:
TPS610986, input 1.5V, output 3.3V, VSUB is followed by a load of 3-5mA,
MODE is low, some VSUBs have charging and discharging waveforms, and some have high levels.
How to understand…