Part Number: TPS61099 Other Parts Discussed in Thread: TPS61033 Is there a Boost Regulator with Integrated MOSFET having Pass-Through Mode for Vin range greater than 5.5V ? I see that Pass-through feature in Integrated MOSFET Boost are available for low…
Part Number: TPS61099 Other Parts Discussed in Thread: TPS61299 , , TPS61033 Hi,
We are newly considering TPS61099 or TPS61299. These are types with variable switching frequency. Could you tell me in what range it can be changed? Or could you please tell…
Part Number: TPS61099 Hi Team,
ON BGA layout.
It says to do this layout where the GND is VIA’d to a large GND plane on bottom side. Understood.
I do have large GND on bottom side, but I also have top side flooded with GND.
Can I let the GND in…
Hi Chi,
I have not seen an update for the last 23 days, so I assume the questions are/or answered and the issue is solved. I close this thread now. If there is still something open reply and the thread will get open again. If you have any other question…
Part Number: TPS61099 I would like to put the outputs (3.5V) of two regulators in parallel.
A TPS61099 with a 3V battery connected to Vin and another buck regulator with a serial diode.
If the buck regulator is powered, it cuts the Enable of the TPS61099…
Part Number: TPS61099 Hi Team,
Can you have a look at the following customer inquiry, please?
We have been using the TPS61099YFFR boost converter in our product for years. This is responsible for supplying an RFID front end from a CR2 lithium-ion battery…
Part Number: TPS61099 Other Parts Discussed in Thread: TPS61299 The datasheet for the TPS61099x family has been updated since the last thread and lists the TPS610991 variant as in preview. I don't see the parts as in preview on the product page anywhere…
Part Number: TPS61099 Dear all,
We have a design with TPS610995 and the LOAD powered from this dc/dc regulator needs that its power supply voltage changes from 0 to 2.1 V in less than 1 ms. As the dc/dc has a softstart and the LOAD needs 100 uF input capacitor…