Part Number: TPS61163A Hi
The device appears to be able to adjust the output current through a resistor connected to the ISET pin, but the typical application in the data sheet uses 63.4 Kohm in all cases. - Can the TPS61163A adjust R_ISET to reduce…
Part Number: TPS61163A Tool/software: Hi,
From the d/s I read the part is actually doing analog dimming with the PWM input signal, but not the real PWM dimming (meaning the LED string current keeps constant but dimmed by PWM chopping
Is this true…
Part Number: TPS61163A Sir,
Please help to check these parts can change tape reel process from self-adhesive sealing film to Heat sealing film.
Thanks!
Part number "TPS61163AYFFR/ LM3644TTYFFR/ TPS63027YFFR /TPD2S300YFFR
Part Number: TPS61163A Tool/software: Howdy experts!
datasheet recommends using a 4.7-10uH inductor, but it mentions that a 22uH inductor can also be used for high current applications and warns about potential stability issues.
7.2.2.1
the best…
Part Number: TPS61163A Dear Sir,
We'd like to use both IFB1 and IFB2 sink channel to apply 40mA current requirement for our one string LED LCM.
Can TPS61163A support this such appliation?
Best regards,
Kevin Chin
Part Number: TPS61163A Other Parts Discussed in Thread: , TPS61165
Hi,
I'm having a strange behavior on a prototype with a TPS61163A.
Schematic:
The problem is that although the datasheet says that the device can operate up to 30 mA per…
Part Number: TPS61163A Hi Team,
As title, I would like to check whether our solution can detect the PWM duty lower than 0.5%. I ask because according by our customer test result, the 0.1% PWM duty avg current was higher than 0.3%/0.2%.
We used…
Part Number: TPS61163A Other Parts Discussed in Thread: LM3508 Dear team,
LM3508 has the feature described in D/S P12"Output Short Circuit Protection". This feature is due to the PFET series to output but is TPS61163A able to support kind of this feature…