Part Number: TPS61165-Q1 Other Parts Discussed in Thread: TPS61165 Hi Team,
Customer now use TPS61165 and found problem in light load. 1: When the voltage after the integration of DISP_PWM is above 1.5V, if there is no-load backlight, the output will continue…
Part Number: TPS61165 While comparing TPS61165 and TPS61165 I came up with the following questions:
1. Why is the CNTRL pin frequency range limited to 6.5kHz min in the industrial version only?
2. Why the 6.5kHz min freq is only mentioned in section 9…
Part Number: TPS61165-Q1 Hi Team,
According to Section 6.3 of the datasheet of TPS61165-Q1, the minimum output voltage (VO) is equal to VIN.
The customer will drive the LED backlight of the TFT LCD at around the maximum drive current of 120mA with all…
Part Number: TPS61165-Q1 Other Parts Discussed in Thread: TPS61500 I want to find a backlight boost chip, 2A or more backlight boost constant current, preferably with TPS61165-Q1 P2P.
Part Number: TPS61165-Q1 Other Parts Discussed in Thread: TPS61165
Hi TI,
Can I use TPS61165 reference schematic(3s9p) below to drive https://www.jetone.com.tw/uploadfiles/327/datasheet/tianma/tianma-panel-tm080tdhg01-40.pdf ?
Is CTRL pin directly controlled…
Part Number: TPS61165-Q1 Dear Sir
We are designing with TI LED driver p/n TPS61165-Q1.
If we don't need PWM/1-wire dimming function, What should we do for CTRL pin ? Pull CTRL pin high ? or Leave CTRL pin floating ? Kindly please advise.
BR,
CCp…
Part Number: TPS61165-Q1 Other Parts Discussed in Thread: TPS61165 , Hi,
TPS61165 has two types of package , SOT23 and WSON.
but regarding TPS61165-Q1, only SOT23 package is available now.
Do you have any plan for TPS61165-Q1 with WSON package?
Thanks
…
Part Number: TPS61165-Q1 Hi,
I have the following circuit below:
When testing the UVLO, I get the following behaviour when approaching the threshold (the below instance is when VIN = 2.27V)
As you can see that the driver appears to start-up and shut…
Part Number: TPS61165-Q1 Hi,
I am currently working on a design and I want to use TPS61165-Q1 to drive backlight.
Here are some requirements:
Input: 9-18V; Output: 350mA Max.
I have designed the schematic as following:
Please let me know if you have any…