Part Number: TPS61169 Tool/software: Hi,
I am design a pcb board, in fact, i'm already finishing designing, and i'm wondering if this inductor will work with the TPS61169.
https://ds.yuden.co.jp/TYCOMPAS/ap/detail?u=M&pn=LSQPA322525T100KR
Any comment…
Part Number: TPS61169 Tool/software: Table 1 in section 2.3 of TI application note SNVA769 , lists the typical input offset voltage for the GM or error amplifier in several TPS611xx backlight driver ICs. The application note gives the typical offset voltage…
Part Number: TPS61169 Other Parts Discussed in Thread: TPS923652 Tool/software: Hi Team,
I have a design challenge due to the provision in the product design to allow users to change LED brightness.
Below is the IR led VI characteristic, user will…
Part Number: TPS61169 Other Parts Discussed in Thread: TPS61199 Dear Sirs,
My customer designed with TPS6169 and had some questions that need help.
Vin: 12V
BL : 80mA*4 / 28V
Cin and Cout use 10uF/50V MLCC
They found
1. there is audible…
Part Number: TPS61169 The TPS61169 datasheet includes recommended inductors, which makes me think that there might be reasons for similar inductors to not be suitable? Specifically, the recommended inductors are not easily available to me so I'm wondering…
Part Number: TPS61169 We are trying to drive some higher current UV LEDs. Based on the data sheet, with a sense resistor of 0.58 ohms we should be getting 352mA
However when measured it is more like 150 mA max.
It appears that there is too much noise…
Part Number: TPS61169 Hi Sir,
My customer asked some questions about the TPS61169, does it support the PWM dimming frequency at 250Hz?
If it can support the 250hz dimming, what is the range of PWM dimming signal duty cycle?
Follow the datasheet…
Part Number: TPS61169 Other Parts Discussed in Thread: TPS92380 Dear TI support team,
I wanted to raised a question about the TPS61169. In the datasheet, it is explain that the minimum dimming value is 1%. We are trying to design a circuit that goes…