Part Number: TPS61169EVM Other Parts Discussed in Thread: TPS61199EVM-598 , TPS61169
Tool/software:
Hi Sir,
My customer verified the driving capacity to connect 2 of TPS61169EVM on display back-light LEDs and found the below issues.
Could you…
Part Number: TPS61169EVM Other Parts Discussed in Thread: TPS61169 , TPS61165 To Whom it may concern :
Currently I am making use of TPS61169 to drive ( single channel ) 6x 6 Leds with Iled 360mA ( application 10.1" LCD backlight driving )
I noticed…
Part Number: TPS61169EVM Hi,
When we connect CTRL to GND to enter shutdown mode, we can still see LED light up a little bit, and the current on LED path is around 5mA. Is it normal?
Thanks!
Antony
Part Number: TPS61169 Other Parts Discussed in Thread: , TPS61160 Hello TI teams,
I am planning to use the TPS61169 to drive the white backlight function of the LCD module.
The LCD module is a 7-inch screen manufactured by Riverdi.
The LCD module…
Part Number: TPS92360 Other Parts Discussed in Thread: TPS61169EVM Tool/software: Hi support team,
It seems that the EVM for the TPS92360 has not yet been released. Is it possible to replace the TPS61169DCKR on the TPS61169EVM with the TPS92360DCKR…
Part Number: TPS61169 Other Parts Discussed in Thread: , TPS61500 Team,
Customer is evaluating TPS61169EVM for IP Camera flashing application in below spec requirement.
Vin: single cell battery 3-4.2V
Iout: 200mA
LED#: 4
Based on customer's…
Part Number: TPS61169 Hi Team,
Our customer would like to use TPS61169 at the following conditions.
[conditions]
-VIN=3.15V
-ILED=20mA
-LEDs=7strings
-PWM = 3.3V, 50kHz, Duty 1% to 100%
So, PWM level(3.3V) is higher than VIN(VIN=3…
Part Number: TPS61169
Hi Team,
We are evaluating TPS61169EVM at the following conditions.
ILED of measurement result does not accord with the calculated value at low PWM duty.
Obviously, we doubt our measurement environment but please let me…