Part Number: TPS61175 Hi there, I just wanted to make sure that I am within the minimum duty cycle for this chip. I was looking at this section on the datasheet 8.2.2.2 Determining the Duty Cycle and calculated my minimum duty cycle of 34% and wanted…
Part Number: TPS61175-Q1 Other Parts Discussed in Thread: TPS61175 I want to discuss the TPS61175 part with a technical expert from TI.
How do I contact them?
Don
Part Number: TPS61175 Dear Team,
The TPS61175PWPR IC model on the website can only be open on SiMetrix.
Could you please help to get the simulation model that can fully compatible with Simplis?
If yes, please drop me a mail(a0235746@ti.com)
BR…
Part Number: TPS61175-Q1
Hi,
I have taken TPS61175-Q1 and made 2 designs. One with output of 12V and one with 24V.
In my board Ill be switching the output voltage between 12V and 24V by putting a resistor in parallel with one of the feedback resistor…
Part Number: TPS61175 Hello I am using TPS61175PWP for boosting voltage from 9-13 V to 12 V.
The input voltage is taken from PV panel which can vary from 9 V to 13 V.
The required output voltage is 12 V.
We are using Typical application circuit…
Part Number: TPS61175 Other Parts Discussed in Thread: PMP11136 Hello. this is my first post for E2E.
my customer request me to prepare OrCAD file for TPS61175 reference circuit for their quick development.
would you mind supporting this request?…
Part Number: TPS61175 Hi team,
My customer have used TPS61175 in their system with 5V input and 29Vout 50mA, this project have mass production for some time, now there is a system change that input voltage is changed to 3.3V.
would you please suggest…
Part Number: TPS61175 Hi there, I wanted to confirm with a specialist that my schematic design is optimal for what I want to do. I used a lot of the information provided from both the datasheet and the TPS61175EVM-326 . My device takes an input voltage…
Part Number: TPS61175 Hi, I'm trying to design a boost converter. I want to know what is the purpose of Enable function in IC TPS61175 . i.e. My Vin = 5V, Vout = 9V ,when enable pin is pull down what will be my Vout at that time whether it is 0V or Vin…
Part Number: TPS61175 Tool/software: WEBENCH® Design Tools Attached is the Webench generated power supply design. I would like to verify for my application of 11.8V to 13.2V input voltage and 30V/300mA output, the components selected work.
The selected…