Part Number: TPS61175 Hi team,
Could you tell me about variation in the Softstart bias current (6uA) and the error amp output clamp release voltage (1.8V)?
Best regards,
Tetsuro
Part Number: LMG1210 Other Parts Discussed in Thread: TPS61175-Q1 , , LM7171 Hello, I have some issues with LMG1210RVRR gate driver. Want to use this IC to switch voltages from 15V to 30V at output of totem pole NMOSFET configuration with bootstrap diode…
Part Number: TPS61175 Team
My customer is looking for a 14V input, isolated 48V output (max 15.4W) boost converter.
There is TPS61175PWPR (~ 18V input, ~ 40V output) and it was written that the flyback can be supported
in datasheet.
Even if it…
Dear Sir,
Yes, turn on the power supply slowly can help to reduce the inrush current. And by the way, use less caps at the output side also helps. But you need to make sure the output caps are enough for the application.
SNVA067C made a mistake. The formula in the TPS61175 datasheet is right. I'll try to found whether I could found the deduced formula for you. Please wait in patience.
Part Number: TPS61175 Hello!
There are differences in SEPIC compensation design equations.
Equations in the snva168e.pdf, p9, Step 9 are different from slva384.pdf, p4
Which variant is correct?
Part Number: TPS61175 Hello team
One of my customer would like to know calculating formula between switching frequency and setting resistor (R4).
The customer also wants to know calculating formula for soft start.
Could you provide the both…