Part Number: TPS61178EVM-792 I am currently making modifications to an evaluation board to boost a 3.6V Li-Ion battery up to 14V-15V. We want an output current of 2A. Due to size limitations, we had to reduce the inductor down to 1uH.
As of now, I am…
Part Number: TPS61178EVM-792 Dear team,
My customer has test our EVM, but they have some questions. Could you please help them? By the way, they change our EVM to 12Vout.
1. There is 8.94V drop when they did load transient from no load to 3A. Is there…
Part Number: TPS61178EVM-792 Other Parts Discussed in Thread: TPS43061 Using the development board, input voltage is 12V from 3 18650 batteries and output is at 16V. Perfect! Just not getting enough current to run our motor. We are using batteries, so…
Part Number: TPS61178EVM-792 Other Parts Discussed in Thread: TPS61178 , TPS61089 , TPS61088 Hi,
So I have here the EVM for the TPS61178. The device is rated to handle voltages as low as 2.7V but the EVM is optimized for
inputs 5V to 12V and a fixed output…