Part Number: TPS61195 Hello,
Our customer use the TPS61195, have a question.
The customer are using the analog dimming mode.
How much the maximum input signal PWM frequency?
Best Regards,
Naoki Aoyama
Part Number: TPS61195 Other Parts Discussed in Thread: TPS61165 Hello
My customer has question about resistor value at FDPWM pin.
In datasheet P3, it is written as follows.
「Place a 43.2kΩ resistor from this pin to AGND programming the internal clock…
Part Number: TPS61195 Hi, Team, We have questions for TPS61195. 1) We want to know the meaning of "DPST mode" Is it possible to change the peak current value of PWM dimming from SMBUS? (Can you control both DUTY and peak current value?) Or will…
Part Number: TPS61195 Hi,
We got a question from the customer about TPS61195EVM-460. Could you help us?
[Question] Could you tell us the part number of following components in EVM?
C1: C2: C3: C4:
Best Regards, tateo
Part Number: TPS61195 Hello,
My Customer are concerned about switching frequency of boost converter.
They hope to use between 680kHz(min) and 750kHz(max).
Because, In their application, it affects the load as noise by doubling or tripling harmonics(NG…
Part Number: TPS61195 Hello,
Make LED back light board using TPS61195 as attached.
Using Analog mode PWM interface, and PWM frequency is 3.9KHz.
Using 16steps of PWM duty cycle (from 4% to 90%)
At the low duty cycle (1 to 4 step : Anode Current 50mA…
Hi Dan,
Yes, correct.
However I'm not sure specific conditions of fault detection in the table is still valid or not - we may need to ask IC design team.
Best regards,
Milo
Other Parts Discussed in Thread: TPS61195 Does the TPS61195 latch fault conditions? If so, can they be cleared any other way besides restarting or toggling enable?
Thanks,
Dan
Other Parts Discussed in Thread: TPS61195 In the TPS61195 datasheet, the mode as set by SEL1/2, is statically set to either GND, VDDIO, or floated. For our application we need the ability to change SEL1/2 based upon end-use. The change is semi-static. That…
Other Parts Discussed in Thread: TPS61195 Hiya,
Considering to use this for a 5V-powered device, however TPS61195-EVM datasheet says minimum voltage for THAT board is 7V.
Since there's nothing else on the evalboard other than TPS61195 itself, which is…