Part Number: TPS61196-Q1 Hi Team,
Our customer wants to use our TPS61196-Q1 in their design, and wants to combine all six PWM inputs to one line to control the dimming as below schematic, can we support this method? Any design concerns for this connection…
Other Parts Discussed in Thread: TPS61196-Q1 art Number: TPS61196-Q1
Hi
My customer had a issue with the TPS61196-Q1 low temperature test.
Temperature : - 20
Issue : TPS61196-Q1 shutdown
Could you review my schematic as attached file.
Part Number: TPS61196-Q1 Other Parts Discussed in Thread: TPS61196 Hi
Below is our application condition. Can you help review our component selection below also is 400KHz switching frequency looks ok?
Also is the junction temperature looks safe?
Architecture…
Part Number: TPS61196 I have used TPS61196 backlight driver IC for LCD display as per below requirement. I am giving 200Hz PWM signal and using 6 channels.I have changed the VOVP threshold value by changing the R3 resistor value to 360k. Also changed…
Part Number: TPS61196-Q1 1. Is it possible to 6 PWM ports are linked together to allow a GPIO port to adjust the light.
2.On page 12,R1+R5=Vstart-Vstop/IHYS,Can you tell me the Vstart and Vstop What does it represent
thank you !!
Part Number: TPS61196-Q1 Dear
our client design TPS61196-Q1, they add TVS connect IFB1-6 to GND.
have any suggestion, or add TVS is not good idea.
TVS P/N D1213A-04V
If any question, Please advise me.
Thanks,
Best rgards,
Lawrence.
Part Number: TPS61196-Q1 hello
we are not easy to get the resistors which has the value of 24.9K and 182K, so we want to use other resistors.
Could you help provide other reference resistors' value for R1, R2 and R5, which are also suitable for the TPS61196…
Part Number: TPS61196-Q1 Other Parts Discussed in Thread: TPS61196 hello
w find Pin 1 shorted to GND.
Is there any impact on the IC pins when choosing the smaller value of resistors comparing the resistors value in datasheet, R149, R150 and R151 as shown…
Part Number: TPS61196-Q1 Other Parts Discussed in Thread: TPS61196 Hello, everyone,
The current use of TPS61196 12V boost to 21V, but when the PWM (500HZ) adjust the brightness of the inductor will be high-frequency sound, how to improve?
Or need to modify…