Part Number: TPS61196-Q1 Other Parts Discussed in Thread: TPS61196 Hello LED Driver team,
My customers asked about the pull-down resistance on EN and PWMx of TPS61196-Q1 as following. On the datasheet, the pull-down resistance is recommended to use 0.8Mohm…
Part Number: TPS61196-Q1 Other Parts Discussed in Thread: TPS61196 , TPS61199 Hi.
Configure the circuit using TPS61196-Q1 and inquire for problems during TEST.
Design
1. We connected the TPS61196 in series with 23 LEDs per Ch.
2. The Ilim setting is…
Part Number: TPS61196 I have used TPS61196 backlight driver IC for LCD display as per below requirement. I am giving 200Hz PWM signal and using 6 channels.I have changed the VOVP threshold value by changing the R3 resistor value to 360k. Also changed…
Part Number: TPS61196-Q1 Dears,
our client spec 27" Panel
input voltage: 10.8v~26.4v
output voltage/mA: 47.6v/ 120mA
Use 2 Channel
For brightness dimming question was can supports 600 steps pulse dimming which determines the LED current (120mA)
It…
Part Number: LM3532 Other Parts Discussed in Thread: LP5520 , LP8860-Q1 , LM3697 , LM3633 , LM3533 , TPS61040 , TPS61042 , TPS61043 , LM3530 , TPS61169 , LM3410 , TPS61176 , TPS61177 , LP8556 , TPS61196 I'm looking at a project that could benefit from having more than…
Part Number: TPS61196 Hey guys,
My switching FET gets incredibly hot and my heat sink has to be massive which makes me think I've done something wrong.
Is it the nature of this architecture? All the heat is in the FET (STP70N10F4 has RdsON 0.0195ohm…
Thank you Patrick.
To add to the data, yesterday I tried a single chip configuration using only one channel (others terminated with 20k per datasheet). There now is a driving waveform at the base of the Q1. The enable pin was connected at ~15s and the…
Part Number: TPS61196 Hi,
We have a backlight driver IC requirement for AUO make panel. Below is the panel specification. I have used TPS61196 backlight driver IC. I am giving 200Hz PWM signal and using 6 channels.I have changed the VOVP threshold value…
Part Number: LP8860-Q1 Other Parts Discussed in Thread: TPS61196-Q1 , LP8864S-Q1 hi,
I'm looking fora 8-ch booster (24Vin to 45Vout) with current sink, 150mA each.
I'm wondering if the LP8860 can be used in M/S topology (like the TPS61196-Q1): if…