Part Number: TPS61200 Other Parts Discussed in Thread: TPS61299 Hello,
for a new project we like to use the TPS61200 with 3,3V output and max. 400mA with an Lithium Cell 1...1,8V max. 2A. The prototype is tested with a laboratory powersupply.
We found…
Part Number: TPS61200 Other Parts Discussed in Thread: TPS61299 Tool/software: Hi
We are using the TPS61200 The VBUS input voltage is from a USB port. The TPS61200 seems to be designed for battery voltage input Is there a 5V output 500mA regulator that…
Part Number: TPS61200 Other Parts Discussed in Thread: TPS62100 , TPS61299 Tool/software: Hi,
We are using the TPS61200 to regulate a 3V7 Lithium Polymer pouch cell (VBATT) to 3V3 to power a microcontroller.
We also have a USB-C connection for flashing…
Part Number: TPS61200 Tool/software: Dear all,
I'm looking in datashhet and it is written thet:
Lmin = Vin x 0.5 (µs/A)
But I'm not able to understant what is µs and A in the calculation.
Can you help me?
Regards,
Ludovic
Part Number: TPS61200 Tool/software:
Hi all,
In one of my projects, I used the TPS61200. The main reason for choosing this IC was UVLO function.
This UVLO behavior has also been confirmed in the following topic: e2e.ti.com/.../tps61200-vout-behavior…
Part Number: TPS61200 Tool/software: Hi expert,
Customer would like to use TPS61200 for battery supply boost to 5Vsys and ORing with a USB 5V supply.
May I clarify with you if TPS61200 can somehow block reverse current e.g. the body diode the B2B…
Part Number: TPS61200 Tool/software: I recently had a circuit manufactured based around the TPS61200, designed to boost the voltage of a single cell rechargeable AAA battery (1.2v) to 3.3v for use in powering a single low current LED.
I have set the…
Part Number: TPS61200 Tool/software: Hello,
I am working with the TPS6120 boost converter and would like to clarify its behavior when the UVLO (Under Voltage Lockout) threshold is triggered.
From my understanding, when VIN drops below the UVLO threshold…
Part Number: TPS61200 Is there a .Lib file for TPS61200 available for Pspice implementation? I can 't seem to find anything for it other than a footprint file.