Part Number: TPS61200 Currently, I´m responsible for a research project. In particular, part of our developed system consist of a ultralow power generator we need to manage.
Our ultralow power generator provides: - Output voltage from 0.4V to 0.9V…
Part Number: TPS61200 Is there a .Lib file for TPS61200 available for Pspice implementation? I can 't seem to find anything for it other than a footprint file.
Part Number: TPS61220 Other Parts Discussed in Thread: TLV61220 , TPS61200 , , TPS61094
Hi,
For our application we need a boost converter whose input voltage should be less than or equal to 2V and greater than 3.5V. The maximum output current can be more…
Part Number: TPS61200 Other Parts Discussed in Thread: TPS61021A I am currently using the TPS61021A in a single AA cell application that requires 4V @ 200mA (max load 5% of the time - probably less than 5mA average) with PMOS reverse battery protection…
Part Number: TPS61200 Hello,
I have a question regarding the TI part TPS61200. In section 10.4.1 the data sheet shows that power save mode is enabled when set low. But the symbol of the part, does not indicate this pin to be asserted when low (active…
Part Number: TPS61200 Hi,
I was trying to test the TPS61200 so I designed and assembled the circuit shown below: Vout=5.5 V. However, I am not getting any output (no voltage) under no load or load conditions. Also, the circuit consumes a lot of current…
Part Number: TPS61200 I want a boost ic which can boost 0.3V input which comes from vibration energy and current with hardly 10mA. Will this product be helpful for me? How should I handle this? Is it enough if I give input voltage to input pin and get…
Part Number: TPS61200 I am making a low power device where I have used TPS61200 which takes input from Lithium Battery (3.5 - 3.7 V) and the desired output should be 3.3V. I have attached the connection diagram above. The output voltage after testing…
Part Number: TPS61200 Other Parts Discussed in Thread: TPS61022 Hi,
This is John from Qmax Systems,
We are designing a product - energy harvesting from solar cell. Our application requires a boost converter to convert 0.5V to 4.2V with an output current…