Part Number: TPS61200 Other Parts Discussed in Thread: TPS61099 We have a product that has been in production for multiple years that use 2 of the TPS61200 boost converters. One is set for a Vout of 3.37V (R1 = 1M, R2 = 174K) output while the other is…
Part Number: TPS61200 Other Parts Discussed in Thread: TPS61022 Hi,
is there any way to increase current limit of TPS61200?. Since the supercapacitors can give more current below 1 volt, it will be very usefull if current limit more than 1.3 A such as…
Part Number: TPS61200 Hi everybody,
i am using the TPS61200 in an application with a low power energy source (less than 1 mA) that is charging a small super capacitor. After charging the capacitor to 0.7 V i want the TPS61200 to power a circuit with…
Part Number: TPS61200 Hi, Could you tell me about out put capacitance and reverse voltage condition. Customers is reading the data sheet below. Customers are considering installing a super cap on Cout to operate somewhat even if the input voltage is off. …
Part Number: TPS61200 I am testing a tps61200 breakout from sparkfun. The UVLO is 3V and the output is 5V. When I connect a 1.5V battery to the input, the output will jump to 5V but fall to 0V immediately( very quick), and it will then output 0V as 1…
Part Number: TPS61200 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models Hi everyone,
Does anyone know where to find the simulation model of the TPS61200 boost converter IC as I want to simulate it before purchasing it.
Also…
Part Number: TPS61200 Other Parts Discussed in Thread: TPS62100 Tool/software: WEBENCH® Design Tools Hi
It was failed when I check this device to operate for the following condition by WEBENCH. Because of current limit and duty cycle limit.
Condition;…
Part Number: TPS61200 Other Parts Discussed in Thread: TPS61089 Hi,
I want to boost-up voltage from 0.4V to 4.2V using TPS61200. I am planning to have separate power rail(3.7V) for Vin and Vaux and source 0.4V connected to inductor and other side of…
Part Number: TPS61200 Other Parts Discussed in Thread: TPS61088 , TPS610987 I've been reviewing the application note for the TPS61200 to use it as a charger with a 0.5V solar cell: http://www.ti.com/lit/an/slva345b/slva345b.pdf . I'm checking to see…