Part Number: TPS61222-EP I'm considering using the above part number boost converter, but am concerned about the output noise at low output currents. In the application, there will be two modes of operation, one at 15 uA, and the other at 150 uA.. The…
Other Parts Discussed in Thread: TPS61222-EP , TPS61240-Q1 , TPS61240 , TPS61222 Would anybody please point me to the right direction where I can find the SPICE model for the TPS61222-EP and TPS61240-Q1 booster.
Thanks, Ali.
Hi Jasper!
I am using the TPS61222EP because it is an enhanced product (EP).
How should I go about verifying the load regulation. Should the maximum load be at 120mA, 5V? I tried to attach such a load and only got a load regulation of 6% and not…
I have a customer who wants to use this device, but needs 2.5V or 3.3V Vout. There does not appear to be an adjustable version available. Can we disclose the values of the internal voltage divider so that the customer could calculate the values for an…
Other Parts Discussed in Thread: BQ24050 , TPS61222 , TPS61222-EP We are using TI’s BQ24050 and TPS61222 for a wearable device as a battery charger and power supply.
J5 is the battery holder and L1 is a 4.7Uh inductor. The problem is that when the battery…