Part Number: TPS61235P Other Parts Discussed in Thread: BQ24195 TPS61235P didn't back to active mode with 100mA
Hi There:
Greeting~ I'd like to need your help to provide some suggestion about our customer who use the TPS61235 & BQ24195 as power bank…
Part Number: TPS61235P I am driving some audio amps at 5vdc and want to use the TPS61235 to step up the voltage from my lithium ion battery pack. The title of the data sheet for the TPS61235 says "8-A Valley Current Synchronous Boost Converters" but the…
Part Number: TPS61235P The part mentioned above does have its feedback connected directly to Vout, and has a Vin between 3.1 to 4.2 and Vout increases and decreases with the change in input voltage and not outputting the 5.1V it is supposed to. attached…
Part Number: TPS61235P Hi Expert,
I saw the datasheet shows the below parameter. Does it mean TPS61235P can support revers protection?
So, it the revers voltage is 5V, the current would be 4+2+2=8uA? Thanks!
Other Parts Discussed in Thread: TPS61235P
Dear Sir/Madam,
We purchased TPS61235P boost up converter that is we got efficiency only 60 % and also have some problems.
1. At 3V input, circuit drawing 1A input current and 380mA output current at 4.8…
Hi Tao,
Thank you for reply,
I answer your question below;
・Vin: 2.9V~4.2V (Li-Ion battery), Vout:5.1V
・Iout: 450mA_normal, 1.5A_Max
Application have audio output, these power is large and need 1.5A.
・Inductor is HER5027-1R0N from Sagami Elec, it maybe…
Other Parts Discussed in Thread: TPS61022 , TPS61094 , TPS61235P Hi.
Need help looking for a suitable part for a new design.
The requirements are as follows:
- No BGA less than 0.7. QFN, DFN preferred
- VIN = 2.8V to 4.2V.
- VOUT = 3.3V. to 3.7V
- IOUT >3…