Part Number: TPS61236P Hi Team,
Our customer would like to use TPS61236P at the following conditions.
This device has the pre-bias function so I would like to know whether this device can start up even if VOUT remains 4.1V.
Could you please let us know…
Part Number: TPS61236P Other Parts Discussed in Thread: TPS61230A , TPS61230 Hi there,
In my customer's application, they are trying to get a 5 V output from an input smaller than but very close to 5 V.
When looking at the datasheet, it says that …
Part Number: TPS61236P Hi,
I posted this morning a post where I explained how I tried to integrate a li ion to 5V @ 2A dc converter using TSP61236P (all resistor and capacitor values come from WEBENCH) and how it didn't work as expected due to my wrong…
Part Number: TPS61236P Hi,
I'm using TPS61236P in order to convert the typical 2.9/4.1V of a li-ion battery to 5V but, after I designed the pcb circuit (all with >10mil traces), the converter output 5V but less than 200mA and the inductance is making…
Part Number: TPS61236P Tool/software: WEBENCH® Design Tools
Hello,
I want to test the IC TPS61236P for my project requirement , while i simulate the reference design it shows schematic in simulation window without load connected also current source…
Part Number: TPS61236P Other Parts Discussed in Thread: TINA-TI Tool/software: Webench Hi Team,
Please check the webench tool startup simulation for the TPS61236P. Under the following design conditions:
Vin=3.9V, Vout(design) =5V Iout(design)=3A, the…
Part Number: TPS61236P Hey
I want to boost the voltage from a lipo battery to about 5V and i need to draw current wit peaks up to maximum 7A (in normal conditions peaks up to 4A)
Does it make sense to link two or more TPS61236P in parallel in order…
Part Number: TPS61236P Hi,
We have a requirement of Boost regulator. We have a Battery with ~3.7V (2.8V - 4.2V range) approx at the input. We want to to boost its voltage to 5V. The current rating required on the output is 3A. It would be good if we can…
Part Number: TPS61236P Other Parts Discussed in Thread: TPS61230A I am using TPS61236P in an application where the input voltage is a LiFePO4 cell. Voltage is from 2.5 to 3.65V. I am switching in loads that with tolerance can range from 1.15 to 1.35 ohms…