Part Number: TPS61240-Q1 Hi Team,
Could you please kindly help to check if TPS61240IDRVQ1 could work with operation TJ=127.8℃, from datasheet, it shows maximum value for operation Tj=125℃. If it is not suitable to use with Tj above 125℃, then do we…
Part Number: TPS61240 Just for confirmation on the tolerance on the feedback resistors:
Quote: The internal feedback resistor is R1=724k, R2=228K, and the reference voltage is VREF=1.2V. but the variation of the resistor is +-14%
So the absolute…
Part Number: TPS61240-Q1 Hi,
As per TPS61240-Q1: Output Current Limit - Power management forum - Power management - TI E2E support forums , the output current supported is upto 240 mA, but simulation shows that the device is unstable (considerable noise…
Part Number: TPS61240 Hi, need your confirmation on body marking on part vs mention in datasheet. I have refer to datasheet but it seem not up to date. 2nd row of receive part is marking code not lot code.
what does 36SI character means? Pls help to…
Part Number: TPS61240-Q1 Other Parts Discussed in Thread: TPS61240 Hello,
I have ordered evolution board of TPS61240 I am testing it using 100mA Load my power supply showing the drawn current is of 160mA I am using Electronic load as a load it can…
Part Number: TPS61240 Hi,
I probably will use the TPS6140 (boost converter) to generate 5V 1W (0.2A) from a single cell Li-Ion battery (4.2V down to 3.0V).
I'm trying to compute the inductor value that I need. Here is my design procedure :
Efficiency…
Part Number: TPS61240-Q1 Other Parts Discussed in Thread: TPS61029-Q1 Hi,
We are using TPS61240-Q1 in our design with input supply as 3.0V. In the updated design we have added additional load and the total load of 5V0 is 281 mA. I would like to know…
Part Number: TPS61240
Hello,
I have some questions about schematic and board layout with TPS61240.
The TPS61240 that I use for my project didn't work property.
I assumed the problem is a board layout, So I updated the layout.
Could you review…