Part Number: TPS61260
Hi All,
I attached files. That is schematics & block-diarams using TPS61260.
+1.8V : 1.8V / 200mA
VDD_S : 1.8V / 100mA
S_PWR_CTR : 1.8V
I want to contol power of Device_1 for power saving.
So, I design like that block-diagrams…
Other Parts Discussed in Thread: TPS61260 , TPS61260EVM-673 Hello, A TPS61260EVM-673 is used in order to evaluate the TPS61260 as a supercapacitor charger. Output voltage was set a 4.0V with R2=143K instead of 182K. Output current limit was set at 30mA with…
Other Parts Discussed in Thread: TPS61260 Hi
I want to power my circuit at 3.3v ( Current requirement max 20 MA) using single or dual alkaline cell. I have selected TPS61260 for this purpose.
so when input is as low as 1V to 1.6 V ( In single Alkaline…
Other Parts Discussed in Thread: TPS61260 , TPS62160
Hi, I want to use the Output over-voltage protection of the TPS61260DRV as a regulating process in my application. I set the output voltage above 4.5 V with the divider (Rp8, Rp9) and charge the ultra…
Other Parts Discussed in Thread: TPS61260 Hello,
I seem to have a unique problem with the TPS61260 part. My application requires running off a CR2032 primary coin cell (3V). I have a TP63030 buck-boost down regulating the battery voltage to supply 2.4V…
Other Parts Discussed in Thread: TPS61260 , TPS63030 Hello,
I seem to have a unique problem with the TPS61260 part. My application requires running off a CR2032 primary coin cell (3V). I have a TP63030 buck-boost down regulating the battery voltage to supply…
Part Number: TPS62160 Other Parts Discussed in Thread: TPS61260 Hi,
TPS61260,
input = 7.5V
output = 3.6V
The circuit was powered up first, then loaded with 200mA. After a few times, the device is damaged and the output voltage become 6.3V. If we lower…