Part Number: TPS61280D Other Parts Discussed in Thread: TPS61280A , Hello,
Is there some supporting documentation that indicates TI offers the TPS61280D as an all-attribute duplicate replacement to TPS61280A. If not, what are the differences between the…
Part Number: TPS61280A Other Parts Discussed in Thread: TPS61281A , TPS61022 The part TPS6128[0-1-2][A-D] is very good and interesting because it's in bypass mode if VIN > 3.3V. But the package 0.4mm BGA is not optimal and can be difficult for PCBA…
Part Number: TPS61280A Other Parts Discussed in Thread: TPS61280D Where can I find line and load transient response data for this part?
Load response I'm interested to characterise is for 40 mA/uS time response, total amount of 2A load transient.
…
Part Number: TPS61280A Hi Team,
Can TI burn the values of the two registers in the TPS61280A ROM before shipment?
CONFIG Register [0x1] MODE_CTRL[1:0] set to "1 0" in TI EEPROM 10: Forced PWM operation.
VOUTROOFSET Register [0x3] default…
Part Number: TPS61280A The circuit is implemented exactly like TPS61280EVM Schematic except that EN, nByp and Vsel are connected to Vin,
It will not start to work through all the input voltage range
Tests done with load, small load and no load at all,…
Part Number: TPS61280A Hi Expert,
We found the product got the leakage issue around 13mA. The processor FAE told us that is known issue. Do you have the document to explain it? How to fix the issue in current PCB? Does the D version will fix it? Thanks…
Part Number: TPS61280 Hi
What is the difference between TPS61280, TPS61280A, TPS61280D? What should I pay attention to when using it? What application is it suitable for?
Thanks
BRs
Elsa Duan
Part Number: TPS61280A In the datasheet it's said:
The TPS6128xA automatically powers-up as soon as the input voltage is applied. The device has an internal soft-start circuit that limits the inrush current during start-up. The first phase in the…
Part Number: TPS61280A Other Parts Discussed in Thread: TPS61280 , Hi Sir,
We plan to use TPS61280 part in our application. The part needs programmed by I2C for Boost threshold at 3V or 2.85V.
A socket board for DSBGA 16 package will be used for every…