Part Number: TPS61287 Hello, I want to increase a 3.2V voltage to 12V using the TPS61287 integrated circuit. I need to draw a maximum current of 3A from the output. I designed the circuit below and had the PCB manufactured, but I get the desired voltage…
Part Number: TPS61287 Dear TI Engineer,
We used TPS61287 to boost the output to 20.8V, but a small number of devices output 26V. At this time, the input voltage of VIN is 12V, and the voltage of FB measured with a multimeter is 1.26V.
The circuit…
Part Number: TPS61287 Other Parts Discussed in Thread: TPS61288
Hello,
My customer is considering using the TPS61287 under the following conditions.
- VIN = 4.2V-3.2V / VOUT = 8V / IOUT = 4A (Max)
Would it be okay to use the external FETs below…
Part Number: TPS61287
Hello All
I have a designed a boost converter with TPS61287. My Vin is supplied from a 12V, 7A PSU and I need a 24V 1.5A at the output. I donot know why it doesnot hold the voltage at 24V when I connect the load. When I measure…
Part Number: TPS61287 Other Parts Discussed in Thread: TPS61372 , TPS61178 Tool/software: Hi Team,
Does TI has solution to prevent current flowback? Currently customer adopt below circuit to achieve it.
Part Number: TPS61287 Tool/software: Hi team,
I'd like to know if Vin is in between 23V to 30V? (and Vout is set to 24V)
Is the internal HS FET bypassed? or turned off?
One of my customer concerned in case of battery ranged 17.4V(min) ~ 25.2V(max…
Part Number: TPS61287 Tool/software: Hello Fergus,
Good day. For TPS61287EVM-042 TPS61287 Synchronous Boost Converter Evaluation Module, is it recommended to have 22uF 25V chip capacitor for a 20V output circuit? Can we replace these 22uF 25V output…