Part Number: TPS61288 Hi Team,
Want to check with you if Vin=8.8V, Iout=2A, what is the min Vout for this operating conditions? Can we use Vout=9V? Thanks.
BRs.
Frank
Part Number: TPS61288 Other Parts Discussed in Thread: PSPICE-FOR-TI TPS61288 PSpice model downloaded from the TI website under the name slvmdh8 is encrypted, while simulating, it is showing error like " C:\Users\vishali.s\Documents\LTspice\Boostckt1…
Part Number: TPS61288 Is there an efficient way to connect two of these circuits in parallel for more output current. My situation is 7.2V in, 15V out. I see this question has been asked a couple of times before, but the answers were taken to private…
Part Number: TPS61288 Tool/software: I am using the TPS61288 to take in a variable input between 3.5- 4.5V at a max supply of 5A and intend to step it up to an output of either 5V, 9V or 12V; I expect a peak current draw of 2A for a 12V load. Basically…
Part Number: TPS61288 Tool/software: Hi, TI expert
I would like to request a schematic review of TPS61288. The specifications are as follows:
- Input Voltage : 3.6V~4.2Vdc (Use battery)
- Output Voltage : 13V~16Vdc
- Output Current : about 10A…
Part Number: TPS61288 Tool/software: Hi Team,
My customer found the output voltage is not 0V while TPS61288 disabled(EN=0)
The Vin=5.28V and Vout=12V.
While EN=1, the Vout=12.5V, but while EN=0, the output still had around 4.9V
Please help to…
Part Number: TPS61288 Hi Team,
in the block diagram of TPS61288, Vout is also connected to the internal LDO, along with Vin. I would to understand what's the design purpose for a boost converter (since Vout is > Vin, using Vout as source actaully decreases…