Part Number: TPS61289EVM Tool/software: Hello Applications team,
Do we have any app notes or guides that show how this device can charge up a supercap with 12V input and then be used in the other direction as a boost up to 12V again in the case of…
Part Number: TPS61289EVM Tool/software: Hi TI expert team,
Could you help to provide the TPS61289EVM altium project files? I would like to creat a new project based on this TPS61289EVM project. Thanks.
BR
Sean
Part Number: TPS61289EVM Other Parts Discussed in Thread: TPS61289 , Tool/software: Hello,
TPS61289 specifies some graphs with VLOW voltages up to 12 V in Boost mode. TPS61289EVM specifies that VLOW can only be up to 5 V.
Given I want a VHIGH of 12…
Part Number: TPS61289EVM Other Parts Discussed in Thread: TPS61289 , TPS61094 , , TPS61299
Tool/software:
Hi TI Team,
I was searching for a bidirectional buck/boost converter with a very low VIN for the backup power, since we like to use only one…
Hi,
will using VLOW side LFP battery in range 2.5V to 3.6V rating and VHIGH side 12V super capacitors( 3V , 4 capacitors in series) ,
The library was issue resolved, could you please provide simulation modal of TPS61289EVM,
TPS61289EVM-113 — TPS61289…
Hi Travis,
Thanks you for your reply.
I was a bit confused on the VFB setting as the datasheet suggest to keep VFB between 0.7V and 0.8V, which is different than the typical methodology of having an accurate VFB reference voltage to set a fixed output…
Part Number: TPS61289 Other Parts Discussed in Thread: LM5155 Tool/software: I am currently testing the TPS61289 on the TPS61289EVM-113 in boost only mode. The datasheet seems to suggest a boost capability of 2 to 15V above 90% at 8 A.
In testing…