Part Number: TPS61291 Hi,
We use a TPS61291 in our design for operating the device from a single LiMnO2 Primary Battery. Now i should design a extension-module that contains the possibility to power the device from a external supply.
If a battery is present…
Part Number: TPS61291 Hi Sir,
I am in charge of a IoT project. I plan to use TPS61291 for main power supply.
Just wondering the current consumption, would you please let me know the maximum output current of the following condition :
VIN : 3.0V ~ 3.6…
Part Number: TPS61291 I am currently using this device in my design.
TI do not have stock available.
Are there a drop in replacement component?
Are there a replacement component that is and will be available?
Thanks
Hi Al,
If you check the product page for TPS61291, you will find an unencrypted model - https://www.ti.com/product/TPS61291
If they are not present on the product page, they are likely not available for distribution.
Regards,
Rahil
Part Number: TPS61291 Other Parts Discussed in Thread: CC1352P Hello,
We are going to use TPS61291 in our design. Please help me with the following question:
How much time does it take to switch from Bypass to Boost mode and vice versa? The EN/BYP signal…
Part Number: TPS61291 Other Parts Discussed in Thread: TPS61099 Hello,
I would like to use the TPS61291 with a LiMnO2 Battery (3V full, 2V near empty). The Device will deliver 3.3V for the Main Application. The battery type we would use, is also available…
Part Number: TPS61291 In one of my projects, I am using buck boost converter from TI # TPS61291.
My power supply voltage is below 2.7V & When I am going to enable boost mode by giving high to enable pin through GPIO (from controller). Its not going in…
Part Number: TPS61291 Hi!
I am working on TPS61291 implementation in our schematics and as far as we understand the EN/BYP must be either LOW or HIGH at ALL times. Our product is using a battery as a power source and when it is inserted - MCU takes time…
Part Number: TPS61291 Other Parts Discussed in Thread: CC1352P Hi Team,
A customer asked the following questions about the EN/BYP pin.
1. Which state should the EN/BYP pin at start-up.
2. Does it matter if EN/BYP pin is at high or low state during start-up…
Part Number: TPS61291 Other Parts Discussed in Thread: TPS610986 , Hello I used both the TPS610986 and TPS61291 boost converter in order to power a load that consume around 200mA in both situation (TPS610986 powering the load then use the TPS61291 to power…