Part Number: TPS61311 Tool/software: The datasheet states that a 220k NTC thermistor should be used. Additionally, the thermistor bias current is specified at 23.8uA. Since the bias is only activated when, for example, video light mode is enabled, the…
Part Number: TPS61311 Hi,
TPS61311 is using the package of DSBGA(20) 2.2mmx1.9mm, but I can't find the number of 2.2mm and 1.9mm in the datasheet at the page of mechanical data. Please let us know from which document we can see this number specified…
Part Number: TPS61311 Hello,
Could I know INDLED can be used to control pin Hi/Lo for below circuit? UFCAM_LED# net connect to LED_Control net.. Thank you.
BR Patrick
Other Parts Discussed in Thread: TPS61311 Hi,
I am planning to use TPS61311 in a down light in continuous mode which would be operating for couple of Hours (6-7 hours everyday ) from a Li-ion battery. From the description what I am able to understand…
Other Parts Discussed in Thread: TPS61311 Hi, I work with TPS61311 and have some problems and questions with programming this module in flash mode. (working with LED2, STRB1 is always = 0)
1. Problem: Video mode is activated after the flash. a) STRB0…
Part Number: TPS61310 Other Parts Discussed in Thread: TPS61311 , LM3643 , LM36011 Hi team,
one of customers is wondering whether TPS61310/TPS61311 is recommended to be mounted on HDI board. From customer's experience, ball pitch under 0.5mm is better…
Hi Victor,
the TPS6132x is designed to drive a higher flash current supported by the super-cap without stressing the battery further.
The typical DC Light Current can be adjusted by the register DCLC13 and DCLC2 and are a bit different for both devices…