Part Number: TPS61322 The TPS613221A (3.3v output) drops the output voltage if Vin goes below 1.28v with a constant 100mA load. Vin 1.28v to 1.5v gives 3.3v out. 1.27v in, out=3.01v. 1.25v in, out 2.94v. 1.2v in, out 2.8v. We tried 2 different inductors…
Part Number: TPS61322 Hi TI Teams,
We found that the two capacitors C70 and C71 can be easily damaged, and returned to normal after replacing them. The following is our schematic of TPS613221A, please help to check if there is any problem in the circuit design…
Part Number: TPS61322
Hi, We are considering using TPS3222A for our new product, implementing a circuit with input voltage : 3.3V output voltage : 5V output current : 200mA
However, I am not quite sure about how to choose a proper inductor. Could I use the…
Part Number: TPS61322 Hello, have a question about TPS61322. I need to get 3.6V (100mA max load). I have two solutions:
1) TPS613226A Use 3.3V input voltage (supplying the CPU) formed by LDO connected to Li-ion battery
2) Use a direct connection to the…
Part Number: TPS61322 I'm using the TPS613222A for my project and am referencing the datasheet for it, particularly figure 24. The data sheet says, in the device comparison table, that the typical current for the chip is 1.8 A. How can I adjust the parameters…
Part Number: TPS61322 Other Parts Discussed in Thread: TPS61021A Webench won't generate a design with TPS613226A - why not ?
Webench recommends TPS61021/22/23 but I would like to use the TPS613226A as it is perfect for my design
My specs are Single…
Part Number: TPS61322 Hi,
We intend to use TPS61322 in an single cell NiMH application that is Vin 1 to 1.5V and Vout 2.2V. I did a test board with the device. The load is 50ohm resistor (100//100) i..e 44mA output current. Input and output capacitors…
Part Number: TPS61322 Other Parts Discussed in Thread: TPS61072 , TPS61090 , TPS61029 Hi Team,
Good day.
Customer is looking for possible alternative for the currently out of stock TPS613221ADBV (3.3V output version).
Customer's requirements:
3.3V output…
Part Number: TPS61322 Hello,
when trying to use the TI WEBENCH for the part TPS613226A with the following input data, I always get an error message that the design cannot be created even though I'm totally within the device limits.
Kind regards…