Part Number: TPS61372 Hello,
How can I calculate TPS61372's input/output voltage ripples from input/output capacitance values?
The "TPS61372 Quickstart Tool" (SLVRBF6) can calculate minimum input capacitance from input voltage ripple spec in the …
Part Number: TPS61372 Hello,
TPS61372's data sheet shows in Figure 8-1 on page 12 1.909 MΩ (upper side) and 100 kΩ (lower side) as feedback resistor divider, and it looks relatively large to me. Is it OK to use lower resistance values for the resistor…
Part Number: TPS61372 Hello,
I would like to ask you about TPS61372. In the board I designed, the A3 pin of this device is left unconnected. The explanation in the data sheet says that this pin is NC, but there is a description that it is connected…
Part Number: TPS61372
Hello Sir
In TPS61372, A3 pin name is NC but description is "No connection .Tie directly to VIN pin" . Should this pin keep No connection or Need tie to VIN pin?
Part Number: TPS61372 Hello,
I would like to ask you about the TPS61372. Specifications are below. I am assuming that a motor will be connected to VOUT, but are there any concerns? Is it okay if the back electromotive force is applied to VOUT?
(Specification…
Part Number: TPS61372 since last update of Excel 365 64 bit the Quickstart Tool is not working any more. The bode plot generates an error and is not displayed. ( Microsoft® Excel® für Microsoft 365 MSO (Version 2208 Build 16.0.15601.20540) 64 Bit )
…
Part Number: TPS61372 Hi,
I have made a design using TPS61372. Attaching the Webench design 6.5V 30mA 85C TPS61372.pdf
Im powering another switcher(LTC3265) using TPS61372. Im concerned about switching current TPS61372 would see from the LTC3265.…
Part Number: TPS61372 Other Parts Discussed in Thread: TPS61376 , TPS61033 , TPS61022 Hello expert,
May we have your help to provide suitable solution to support 3.3V -> 5V/2A and 12V/0.5A condition? also my customer needs true shutdown function when…