Part Number: TPS61377 Other Parts Discussed in Thread: TPS61376 , TPS61178 Dear Sir
We are using the TPS as step up. Our input voltage is 14V and output is 20V. We are charging a capacitor using its output and after that its TPS71377 function should…
Part Number: TPS61178 Other Parts Discussed in Thread: TPS61377 , TPS61287 Tool/software: Hi Team,
Can you share the efficiency of TPS61178 when Vin=3V, Vout=20V. Iout=0.8A?
Besides, how do you think the efficiency of TPS61178 in this condition…
Part Number: TPS61170 Other Parts Discussed in Thread: TPS61376 , TPS61377 Hello,
I need 15V power supply for a small OLED panel (around 120 mA max when all pixels are on) from Vin=12V. I am looking to minimize output voltage ripple because it can be…
Part Number: TPS61376 Other Parts Discussed in Thread: TPS61287 , TPS61377 Hello Team,
We are designing the boost converter circuit with below parameters:
VIN: 5V
VOUT: 20V, 0.5A(Nominal Current), 1.6A(Peak Current)
Please share the calculation…
Part Number: TPS61175EVM-326 Other Parts Discussed in Thread: TPS61377 I am using the EVM board to validate the specifications. The target specifications are V_in = 3.0 V, V_out = 24 V, and I_out = 250 mA . However, this load requirement is not being…
Part Number: TPS61383-Q1 Other Parts Discussed in Thread: TPS61377 Dear TI Support Team,
My name is Jongyoon Chae, and I am a Ph.D. student at the Georgia Institute of Technology conducting research in power electronics.
We are currently developing…
Part Number: TPS259827LEVM Other Parts Discussed in Thread: TPS61377 Tool/software: Dear Sir
Vin=19V,Vout=24V,Iout=3A
Solution:TPS61377+TPS259827LEVM
Problem:It not have 24V output,when power on at 3A
As below is fine-turn location at EVM…
Part Number: TPS61089 Other Parts Discussed in Thread: TPS55340 , TPS61377 Hi All.
i am using item TPS55340QRTERQ1 the item rgultates from 5v to 12v , but cannot rgulate well the 12v output,this is being caused probably due to the currrent peaks it…
Part Number: TPS60150 Other Parts Discussed in Thread: TPS61287 , TPS61377 Tool/software: Hi
Could you help suggest suitable products It is necessary to boost 5V to about 20V (or 12V to about 20V) to control the 12V input N-MOSFET
Thank you
Part Number: TPS61376 Other Parts Discussed in Thread: TPS61377 Tool/software: Hello, I've gotten somewhat confused on the compensation network calculations for the TPS61376. It seems following the datasheet example doesn't yield the component values…