Part Number: TPS61377EVM Tool/software: Hi Team, My customer has a critical project and we want to promote TPS61377RYHR in this project. They need the EVM's schematic and PCB source document (Altium PCB project) which can help to finish the project design…
Part Number: TPS61377EVM Tool/software: Using this EVM it appears short circuits on the output cause destruction of the IC, yet the data sheet states cycle by cycle current limit protection.
Part Number: TPS61377EVM
Tool/software:
Hi team,
I want to use this EVM to achieve 6A output current, however, the default current is 1.5A.
What changes do I need to make on this EVM? Change the inductor to meet the Isat?.
Vin: 12V-16.8V(4s3p)
Vout:…
Part Number: TPS61377EVM Hi,
As the TPS61377EVM user guide, the input voltage range is 9V to 16V, but the IC and input caps are rating over 20V, may I use 19V for input?
Suppose it is okay, just double check.
Thanks and Best regards,
Tiger