Part Number: TPS61378-Q1 Other Parts Discussed in Thread: TINA-TI Tool/software: Hi, please help me with this
I want to import the TPS61378-Q1 to TINA-TI , PSpice Downloadable file is present on website of TPS61378-Q1
Please share the steps or the TINA…
Part Number: TPS61378-Q1 Other Parts Discussed in Thread: TINA-TI Tool/software: Hi, there is an updation on the above question.
I am able to import the PSPICE model to TINA - TI,
TPS61378-Q1, in the downloadable files, encrypted version is available…
Part Number: TPS61378-Q1 Tool/software: Hi team,
when test TPS61378EVM, with 0.5A load, 5V output, when increase Vin from 3.3V to 4.2V, the device enter into down mode (OUT pin is 6.14V). Then customer decrease Vin to 3.63V , but device didn't exit down…
Part Number: TPS61378-Q1 Tool/software: Team,
Currently my customer finds that there is one TPS61378 no output. The input voltage is 7.7V and normal board output voltage is 125V. On one board, we find that the Vout=0 and OUT=8V, SW output is good and…
Part Number: TPS61378-Q1 Tool/software: Hi Team,
Currently We are using TPS61378-Q1 Booster in our design.
Vin(VBAT_INT) - 2.3 V to 4.1 V(Vin Source from Li ion battery)
Vout - 5.2 V
In datasheet its mentioned, Rising EN threshold voltage is approx 0…
Part Number: TPS61378-Q1 Tool/software: Hi team,
While testing TPS61378-Q1 Booster IC, come across following observations.
Booster output voltage is dipping even though Input voltage is stable and peak current limit is within the limit.
Input Voltage…
Part Number: TPS61378-Q1 Tool/software: In my application the inductor temperature is about 30°C over the ambient temperature also without load..
Can you help me?
Part Number: TPS61378-Q1 Tool/software: Hi ,
When TPS61378 was simulated in the Web bench tool for the input requirements: Vin =5V, Vout=9V, Iout=1A, the results of the design were obtained as attached. The ripple current percentage mentioned is 43.664…
Part Number: TPS61378-Q1 Hi Team,
We are currently using TPS61378-Q1 Booster IC in our design.
We are Validating TPS61378-Q1 for below Voltage and load condition,
Vin = 2.3 V to 4.1 V
Vout = 5.25 V
Max load current =1.5 A
Observation:
Upon reaching…
Part Number: TPS61378-Q1 Tool/software: We are considering a circuit with an input voltage of 9V and an output voltage of 12V. If the output voltage setting is 12V and the input voltage is higher than 12V (e.g. 13V), what will happen to the output voltage…