Part Number: TPS61378-Q1 Tool/software: Team,
Currently my customer finds that there is one TPS61378 no output. The input voltage is 7.7V and normal board output voltage is 125V. On one board, we find that the Vout=0 and OUT=8V, SW output is good…
Part Number: TPS61378-Q1 Tool/software: Hi team,
I have designed the following boost converter schematic to accept a regulated 5V at 2A to output 12V at 0.7A max. Can you check the schematic to ensure the passive values are right, and if the input power…
Part Number: TPS61378-Q1 Tool/software: Hello,
I used TI's Web-Bench to design a circuit that uses the TPS61378-Q1 and that takes 4.2 VDC from a single cell Li-ion battery and boosts it to 12 VDC with the enable pin high in accordance with the schematic…
Part Number: TPS61378-Q1 Other Parts Discussed in Thread: TPS61033-Q1
Hi Team,
Kindly Review the attached Schematic circuit for TPS61378-Q1 and provide the feedback
Below mentioning the design details,
Input Voltage - 4.1V(Max) and 2.3V (Min)…
Part Number: TPS61378-Q1 Hi Team,
The Query is regarding TPS61378-Q1 Booster,
In PFM mode, upto 100uA load current,booster output voltage will get regulated.(Attaching plot from datasheet below)
Mentioning below our design condition,
a)Vin=4…
Part Number: TPS61378-Q1 Tool/software: Hello,
I'm using the TPS613785 and am trying to achieve an output of ~13V from a battery input of 3.8V. Regardless of the feedback resistor conf, I'm only 11.9V at the output. I'm able to adjust it to values below…
Part Number: TPS61378-Q1 Hi team,
TPS61378-Q1 SW voltage range is -0.3V to 23V as below in datasheet. But our test result is much lower than -0.3V when check the undershoot. the pulse width under -0.3V is very short, refer to below measurements. Is…
Part Number: TPS61378-Q1 Hello experts.
I'm planning to use the TPS61378-Q1 for circuit design and have a few questions.
1、Input voltage range 9~12V, output voltage 12.5V, maximum current 0.5A, Input voltage remains at 12V in most cases.using TPS61378…
Part Number: TPS61378-Q1 Other Parts Discussed in Thread: LM7310 Dear Madam, Dear Sir,
we’re using the TPS61378-Q1 in a new design to drive a load of around 300..400uF at around 15Ohms, Vin=5V, Vout=6V, Inominal=500mA.
Unfortunately the load current…