Part Number: TPS61378-Q1 Hello experts.
I'm planning to use the TPS61378-Q1 for circuit design and have a few questions.
1、Input voltage range 9~12V, output voltage 12.5V, maximum current 0.5A, Input voltage remains at 12V in most cases.using TPS61378…
Hi Yufang,
Thank you for your feedback.
According to your three different simulation results, although the TINA one seem a little ideal, you can refer to its results. The conclusion we verified on the TI EVM is that TPS61378-Q1 can achieve stable operation…
Part Number: TPS61378-Q1
Hello,
I used the same circuit and read the SW waveform. I found the result trend of SIMPLIS software is different from " PSpice for TI" and "TINA" . There should be a slow-start switching frequency between 0ms…
Part Number: TPS61378-Q1 Following is the requirement in my application:
Input Voltage: 2.3V to 4.1V
Output Voltage: 5.5V
Maximum Output Current (Maximum Load Current): 0.6A
When ripple percentage is considered around 40 percent of Input current, the…
Part Number: TPS61378-Q1 Hi expert,
When I was doing a power test, I found that the output does not turn off under a large current load, but a voltage drop occurs. I want to calculate the turning point of the V-I curve and the short-circuit protection…
Part Number: TPS61378-Q1 Dear TI Expert,
I would like to use TPS61378-Q1 with Vin=12V and Vout=17V.
If the above case, how much can load output current?
I'm appreceate if answer.
Part Number: TPS61378-Q1 Dear TI expert,
We tested the TPS61378 in our project. Please help check SW voltage overshoot and undershoot issue as below.
Defines -0.3v in datasheet, but it is -2v in test waveform. Whether can it be accepted? What's the judgment…
Part Number: TPS61378-Q1 Hi Team,
When using a 5V0 fixed output by tying a 0ohm resistor to ground per datasheet:
What Rbottom/Rtop should be used for plugging into the design calculator? Typing in 0ohm gives a flat bode plot.
Thanks!
David
Best,
D…
Part Number: TPS61378-Q1 Hi Expert,
Do we have the average model for TPS61378-Q1 to perform Monte carlo, Loop response for 8V5 Boost supply?
I have found the PSPICE transient model on ti.com.
Thanks!
Ethan Wen