Part Number: TPS61500 Tool/software: We are looking for an LED driver with the following specification: Vin 3 to 12, better 20V. Vled 22V with 100 mA current. The backlight should be controlled via PWM. The decisive criterion is a low duty cycle so that…
Hi Liang,
I have setup the EVM with similar condition, the IC still works normally. May I know if customer could also send me their layout for double check? You can send it to me through private message if customer has confidential concern.
BR
Patric…
Part Number: TPS61500 Tool/software: Hello Support team,
I am going to design backlight driver for 14.5-inch display to supply current to WLED Backlight consists of 5 strings with 8 LEDs for each string.
The backlight has common anode and common cathode…
Part Number: TPS61500 Tool/software: Hi champs,
My customer has been using TPS61500 in PWM dimming mode with a PWM from MCU connected to EN pin.
In the new design, they are considering to cancel the MCU, and they do not need any dimming. Can they just…
Part Number: TPS61500 Other Parts Discussed in Thread: TPS61169 , , TPS92360 We have a 3V (700mA) LED, which needs to be modulated from 100Hz to 2MHz with a 50% duty cycle (square wave). I wannted to enquir if the above driver (TPS61500) will work. Also would…
Part Number: TPS61500 Tool/software: Hello team,
On the datasheet, it is stated that Max duty cycle is 93% (TYP).
What is deciding this max duty cycle?
Is it decided by the max duty cycle of the low side FET?
Best Regards, Kei Kuwahara
Hi Conor,
TPS61500 can handle the LCD 1~3 separately, you can adjust R3 in datasheet typical application schematic for different LED current.
BR
Patrick
Part Number: TPS61500 Hi,
We are using TPS61500 IC for my 7 inch LCD Backlight . Below is the panel details. We have provided the 5V as input to the IC. We are facing the issue of LCD flickering some times. What could be the reason for backlight flickering…
Part Number: TPS61500 Hi,
From the datasheet of TPS61500 (SLVS893F –DECEMBER 2008–REVISED MAY 2019), it states in the beginning that
3-A, 40-V Internal Power Switch – Four 3-W LEDs From 5-V Input – Eight 3-W LEDs From 12-V Input …