Hi Alex,
TPS62840 belongs to another team, I'll loop them for this data support.
In the meantime, you can take TPS62150/TPS62050 into consideration.
The maximum input current of TPS62150 under 0uA output current is 785uA when it runs into 100% duty…
Part Number: TPS62050 Other Parts Discussed in Thread: TPS62147 Hi, Customers use TPS in fixed PWM mode. Can the sync pin be connected directly to VIN? Is pull-up resistor required? Best Regards, Yusuke/Japan Disty
Part Number: TPS62050 Other Parts Discussed in Thread: TPS62160 Hi, Could you tell me about TPS62050 power save mode? When using different lot devices, PFM mode sometimes occurs in same circuit and parts conditions. For that reason, I am investigating what…
Part Number: TPS62050 Hi,
On pg.15, section 10.2.1.2.4, it mentions "The converter enters the fixed frequency PWM mode again as soon as the output voltage falls below the
comparator low 2 threshold set to 1.6% below V O , nominal. ". Is this happens…
Other Parts Discussed in Thread: TPS63000 , TPS62050 Hi Team,
We use the T PS63000 Vin: 4.2V and Vout: 5V to measure the output inrush current with Cin: 10uF and Cout: 47uF.
The test result show as below.
And
We use the T PS62050 Vin: 4.2V and Vout: 2.7V to…
Other Parts Discussed in Thread: TPS62050 , TPS62160 , TPS62150 , TPS62175 , TPS62125 Hi,
I wanted to know the instantaneous maximum voltage rating for the Vin PIN of the TPS62050 IC.
regards,
Praveen
Other Parts Discussed in Thread: TPS62110 , TPS62050 , TPS62160 , TPS62140 About the parasitic diode of TPS62110 and TPS62050, if it has spec., please let me know.
I would like to know the spec(voltage and current) of a parasitic diode as reference when reverse…
Sorry, I should have detailed the problem better.
The microcontroller is not powered by the output of this chip. It is powered by a separate 5V supply, and TPS62050 is used to power another device. The EN pin is connected to a digital I/O pin of the…
Other Parts Discussed in Thread: TPS62050 , TPS62056 , TPS62160 Hello
in an earlier revision we were using the TPS62056 (3.3V fixed output). Now we switched to the version with adjustable output TPS62050. We are using the switch converter with a external…